This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH949-Q1: Disable HDCP to work with UB Serializer

Part Number: DS90UH949-Q1


Hello,

My customer would like to source DS90UH940N-Q1 in place of the DS90UB940N-Q1 to keep production running. Their product is already in production and paired with a DS90UB949-Q1 Serializer.

  1. Can the HDCP function be disabled on the UH940N and work with the non HDCP UB949 Serializer
  2. Is the UH940N compatible and is it still under warranty when connected to a UB Serializer in production?
  3. Can you confirm the Ux940N devices are P2P with no HW changes?

Kind regards

Dierk Bronner | Staff FAE Automotive

Office: +49 711 7704 224