Part Number: TLK2711-SP
What is the maximum junction temperature for this device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK2711-SP
What is the maximum junction temperature for this device?
Hi Joey,
Unfortunately I don't have any quality data related to the max junction temperature. I think we could estimate a max junction temperature using the Junction-to-case thermal resistance, max power consumption, and max case temperature.
125C + (2.96C/W * 0.550W) = 126.6C.
I'd assume there's probably a bit of a buffer on the max junction temperature from this value.
Thanks,
Drew
In theory, 150 °C; see [FAQ] What is the maximum junction temperature (TJMAX) for a device?
In practice, the Tc and PD limitations prevent you from reaching that value.