Part Number: TS3DV642-Q1
HI EXPERTS ,
I HAVE DESIGN THAT I USE THIS MUX AS MIPI MUX.
1. AT THE EVB OF TI RELATED TO THIS MUX ALL THE DATA LANES ARE CONNECTED TO 0.22U CAPACITOR DOES IT NECESARY?
2. AT THE EVB, THE MUX OUTPUT LANES ARE CONNECTED WITH 0 OHM RESISTOR TO VCC WHAT IS THE PERPUSE SHOULD I DO THE SAME IN MY DESIGN?
3. PINS THAT ARE NOT USED LIKE SCL , SDA TO LEAVE IT FLOAT OR CONNECT THEM TO GROUND?
4. IN MY DESIGN GROUP "A" IS 4 LANES WITH 1 CLK , GROUP "B" IS ONLY 1 LANE AND 1 CLK, WHAT SHOULD I DO WITH THE 3 LANES (B1+-,B2+-,B3+-) THAT I ARE NOT USED?
THX,
AMI