Part Number: THVD8000
Other Parts Discussed in Thread: TPS62A01
THVD8000接続について質問です
I have a question about THVD8000 connection
添付ファイルを見て下さい
Please see attached file
電源はTPS62A01を使用します
Power supply uses TPS62A01
Fig1はSingle ended connectionです
Fig1 is Single ended connection
①この接続図で間違っている場所はありますか?
Is there anything wrong in this connection diagram?
②この接続でTHVD8000は動作しますか?
Will THVD8000 work with this connection?
③この接続でMCUに電源は供給されますか?
Does this connection supply power to the MCU?
④この接続でTPS62A01を使用できますか?
Can I use the TPS62A01 with this connection?
Fig2はDifferntial connectionです
Fig2 is Differential connection
⑤この接続図で間違っている場所はありますか?
Is there anything wrong in this connection diagram?
⑥この接続でTHVD8000は動作しますか?
Will THVD8000 work with this connection?
⑦この接続でMCUに電源は供給されますか?
Does this connection supply power to the MCU?
⑧この接続でTPS62A01を使用できますか?
Will THVD8000 work with this connection?
thank you.