Part Number: TIC12400-Q1
Other Parts Discussed in Thread: TIC12400,
Hi Team,
The requirement for the resistor coded switch to be interfaced with the MSDI is as follows:
- 10K when switch not pressed
- Press to Ground when the switch is active.
and the wetting current requirement is 10mA during active state. Now when the switch is not pressed the voltage red at the INX pin would be (10mA*10K) which is 100V and this would obviously violate TIC12400 input voltage range.
Is this (simple) consideration correct, or is there any other/better way to have TIC12400-Q1 bias and read the switch values?