This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
One of our customer's issues, I'm forwarding it below, could you please provide your support
There are four EDID configurations:
1、We choose the first scheme External local EDID (EEPROM).
The selected EEPROM chip model is BR24T128-W, the package is DIP-T8, 128K memory (16K*8), 1.6V~5.5V power supply, and the highest frequency of IIC is 400KHZ. Please check with TI to see if it applies.
2、The configuration of MODE_SEL [1:0] is as follows: please confirm whether the configuration is correct
EDID_SEL: 1
AUX_I2S: 0
EXT_CTL: 0
COAX: 0
REM_EDID_LOAD: 0
J10 is an HDMI interface, and now there are the following questions:
1) Whether the 929 chip can read and write the external EEPROM
2) Whether the EDID information in the EEPROM is directly read by the host through the HDMI interface, or is the EDID information in the EERPROM read first through the 929 chip and then sent to the host
3) In what format is the EDID information stored in the EEPROM
Best Regards,
Amy Luo
Hi Amy,
I will look into this and get back to you in 1-2 days.
Regards,
Ben
Hi Amy,
Please check with TI to see if it applies.
I am not familiar with this particular device, but it seems the package type and bit format are correct for our EVMs.
1) Whether the 929 chip can read and write the external EEPROM
When connected to the DCC lines of the HDMI input as is the case in our EVM, the 929 cannot read or write to the external EEPROM
2) Whether the EDID information in the EEPROM is directly read by the host through the HDMI interface, or is the EDID information in the EERPROM read first through the 929 chip and then sent to the host
In the case I described above, the EEPROM is read by the host through the HDMI interface. The 929 never receives information directly from the EEPROM.
3) In what format is the EDID information stored in the EEPROM
Can you clarify what you mean here? There is an example of EDID data in the 929 datasheet (Section 7.3.4.4) that may help you to understand this format. Other specific addressing information would be found in the EEPROM datasheet.
Regards,
Ben
Hi Ben,
Thank you very much for your response. The customer has additional questions:
1: Whether the MOD_SEL switch controls the selection of DDC_SDA and DDC_SCL links.
2: After setting MOD_SEL, when HDMI reads data, it is found that there is an error in the data, it seems that both 929 and EEPROM have responded to it. Whether the MOD_SEL setting is invalid.
3: How to realize the point-to-point communication between HDMI and EEPROM.
Best Regards,
Amy
Hi Amy,
1: Whether the MOD_SEL switch controls the selection of DDC_SDA and DDC_SCL links.
Not directly, but EDID_SEL determines whether an external local EDID is used. In this case, the DDC lines are used to communicate with the EEPROM.
2: After setting MOD_SEL, when HDMI reads data, it is found that there is an error in the data, it seems that both 929 and EEPROM have responded to it. Whether the MOD_SEL setting is invalid
I think the MODE_SEL settings you provided previously are correct based on the setup you have described. Registers 0x4F (BRIDGE_CTL), 0x50 (BRIDGE_STS), and 0x51 (EDID_ID) would be helpful to understand the error that is occurring.
3: How to realize the point-to-point communication between HDMI and EEPROM.
I am not sure I understand what you are asking here. Can you elaborate?
Regards,
Ben