Part Number: DS90LV804
Other Parts Discussed in Thread: ISO7820LL
I wanted to know how many mA the Tx of this component (DS90LV804) has?
Also is there such component (with the same drive strength) and offers data isolation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
All LVDS drivers must be able to generate a voltage drop of at least 250 mV over the 100 Ω termination resistor. This is specified as VOD.
There are LVDS isolators like the ISO7820LL. If you need more than 100 Mbps, combine LVDS receivers/transmitters with plain digital isolators, but those do not go above 150 Mbps.
Clemens, thanks.
All LVDS drivers must be able to generate a voltage drop of at least 250 mV to 454mV over the 100 Ω termination resistor.
Thanks
David