Part Number: DS160PR421
Do we need external termination or AC coupling CAP for connecting data lane of DS160PR421RUAR to DS160PR421RUAR?
Thanks
Francis
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS160PR421
Do we need external termination or AC coupling CAP for connecting data lane of DS160PR421RUAR to DS160PR421RUAR?
Thanks
Francis
Hi Francis,
It is best practice to include AC coupling capacitors on the Tx outputs near the connector or Rx of the receiving device. There is no external termination needed.
Regards,
Nicholaus
Hi Nick,
This is Tx DS160PR421 to RX DS160PR421. The datasheet doesn't require AC coupling.
Thanks
Francis
Hi Francis,
I understand. While it may not be in the datasheet, it is in the PCIe standard for Tx to have AC coupling capacitors.

If you do not want to add them, then it will probably be OK; however, it is best practice to add AC coupling caps to ensure common voltage is the same and to be compliant with the PCIe specification.
Regards,
Nicholaus
Hi Nick,
The issue is we configure it with boot trap correctly for MUX function with PCIe disable.
We have input data, but we don't see the output.
Thanks
Francis
Hi Francis,
I can address the question about the configuration of the MUX in your other post: (+) DS160PR421: DS160PR421RUAR - Interface forum - Interface - TI E2E support forums
I see, thank you for the clarification; however, DisplayPort specification also requires AC coupling capacitors on the Tx lines. So it is still best-practice to have AC coupling capacitors on the output of the redriver, even though it may work without it.
Regards,
Nicholaus
Thanks Nick,
I will add AC coupling in next spin.
For now, I don't know why I don't see output.
Thanks
Francis
Hi Francis,
Sounds good. My first guess is that it this is related to the Rx Detection circuit, but as you said, it should be disabled. Let's talk about this issue in your other post. I will consider this one resolved.
Regards,
Nicholaus