Part Number: TUSB2E22
Hi Sir:
Please find the attached is the USB2.0 repeater schematic PDF file.
Please help review TUSB2E22YCGR schematic and kindly revise.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB2E22
Hi Sir:
Please find the attached is the USB2.0 repeater schematic PDF file.
Please help review TUSB2E22YCGR schematic and kindly revise.
Thank you.
Hello,
I'm reviewing the schematic and will complete it within 24 hours.
Regards,
Nicholaus
Hello,
Here is the completed review:
TUSB2E22 Review (U3501)
High Speed Differential I/Os
eD0/eD1: OK
DA/DB: OK
Control
RESETB: OK, 1K pullup to 1.8V. Open drain control.
CROSS: OK, Directly to GND, Low.
RSVD1: OK, 1K to 1.8V, High.
RSVD2: OK, 1K to 1.8V, High.
RSVD3: OK, Floating.
EQ0: OK, 10K to GND, Low.
EQ1: OK, 10K to GND, Low.
Power
VDD3V3: OK, 0.1uF decoupling caps at each pin.
VDD1V8: OK, 0.1uF decoupling caps at each pin.
Regards,
Nicholaus