Part Number: DP83TG720EVM-MC
Other Parts Discussed in Thread: DP83TC812EVM-MC
Hi
I'm using two DP83TG720EVM-MC one configured as Master other as slave ( header pin placed 1-2 on one & 2-3 on other).


So according to datasheet I should see D2 light up when link is down. D3 light up when link is established(master) and D4 light up when link is establish(slave).
However I see D2,D3 light up on master board & D2,D4 light up on slave board. Isn't that contradictory ? As if the two boards are recognizing each other as master and slave then link is established and D2 should be off ?
Thanks