Part Number: DS90UB960-Q1
Hi team,
One of our customer's issues, I'm forwarding it below, could you please provide some troubleshooting suggestions
In actual use, the customer found that when the video was output of 1280*720p_yuv422_8bit@30fps, the DS90UB960-Q1 would output 4 additional columns of data for a total of 1284*720 data.
The above problem still exists when using the DS90UB960-Q1 test pattern.
The test mode initialization code is as follows:
0x32,0x01, //CSI0 select
0x33,0x03, //CSI_EN & CSI0 2Lane,BIT[5:4] controls lane count
0x21,0x83, // replicate port 0 to port 1
0x20,0x00, //e0//forwarding of RX0 to CSI0
0x1f,0x02,
0x4c,0x01,//
0x6E,0xAA, //BC_GPIO_CTL0: FrameSync signal to GPIO0/1
0x10,0x91,
0x58,0x58, //enable pass throu BCC_CONFIG Register:BACK Channel config
//0x19,0x01, //FS_HIGH_TIME_1
//0x1A,0x15, //FS_HIGH_TIME_0
//0x1B,0x09, //FS_LOW_TIME_1
//0x1C,0xc2, //FS_LOW_TIME_0
//0x18,0x01, //Enable FrameSync
//0x19,0x01, //FS_HIGH_TIME_1
0x1A,0x06, //FS_HIGH_TIME_0
0x1B,0x5b, //FS_LOW_TIME_1
0x1C,0x9b, //FS_LOW_TIME_0
0x18,0x43, //Enable FrameSync
//0x1f,0x02,
0x6d,0x7f, //Configure port to coax mode and FPD III to CSI mode
0x5c,0xb0, //7-bit Remote Serializer Alias ID TX_ID
0x5d,0x60, //7-bit Remote Slave Device ID 0 Sensor ID
//Sensor physical ID
//Configures the physical I2C address of the remote I2C Slave device
//attached to the remote Serializer. If an I2C transaction is addressed
//to the Slave Alias ID3, the transaction is remapped to this address
//before passing the transaction across the Bi-directional Control
//Channel to the Serializer.
0x65,0x60, //7-bit Remote Slave Device Alias ID 0 Sensor Alias ID
//Configures the decoder for detecting transactions designated for an
//I2C Slave device attached to the remote Serializer. The transaction
//is remapped to the address specified in the Slave ID0 register. A
//value of 0 in this field disables access to the remote I2C Slave.
0x70,0x1e, //RAW10_datatype_yuv422b10_VC0
0x7c,0xe1,
0xB0,0x00,
0xB1,0x01,
0xB2,0x01,
0xB1,0x02,
0xB2,0x33,
0xB1,0x03,
0xB2,0x1e,//yuv8bit
0xB1,0x04,
0xB2,0x0a,//1280*2
0xB1,0x05,
0xB2,0x00,
0xB1,0x06,
0xB2,0x01,
0xB1,0x07,
0xB2,0xE0,
0xB1,0x08,
0xB2,0x02,
0xB1,0x09,
0xB2,0xD0,
0xB1,0x0A,
0xB2,0x04,
0xB1,0x0B,
0xB2,0x1A,
0xB1,0x0C,
0xB2,0x0C,
0xB1,0x0D,
0xB2,0x67,
0xB1,0x0E,
0xB2,0x21,
0xB1,0x0F,
0xB2,0x0A,
0x20,0x00, //e0//forwarding of RX0 to CSI0
-------------------------------------------------------------
As the code shows, the configured test mode output is yuv4228bit of 1280*720.However, the upper computer software must be configured to 1284*720 parse the image to get a correct image, and there is a noticeable column of anomalies to the right of the image, as shown in the following figure.

If I use 1280 * 720 to resolve, I get an image like this:

What's more interesting is that I'm adjusting the test pattern output data to a yuv output of 1200x720, and that's not the problem.The code changes are as follows
0x32,0x01, //CSI0 select
0x33,0x03, //CSI_EN & CSI0 2Lane,BIT[5:4] controls lane count
0x21,0x83, // replicate port 0 to port 1
0x20,0x00, //e0//forwarding of RX0 to CSI0
0x1f,0x02,
0x4c,0x01,//
0x6E,0xAA, //BC_GPIO_CTL0: FrameSync signal to GPIO0/1
0x10,0x91,
0x58,0x58, //enable pass throu BCC_CONFIG Register:BACK Channel config
//0x19,0x01, //FS_HIGH_TIME_1
//0x1A,0x15, //FS_HIGH_TIME_0
//0x1B,0x09, //FS_LOW_TIME_1
//0x1C,0xc2, //FS_LOW_TIME_0
//0x18,0x01, //Enable FrameSync
//0x19,0x01, //FS_HIGH_TIME_1
0x1A,0x06, //FS_HIGH_TIME_0
0x1B,0x5b, //FS_LOW_TIME_1
0x1C,0x9b, //FS_LOW_TIME_0
0x18,0x43, //Enable FrameSync
//0x1f,0x02,
0x6d,0x7f, //Configure port to coax mode and FPD III to CSI mode
0x5c,0xb0, //7-bit Remote Serializer Alias ID TX_ID
0x5d,0x60, //7-bit Remote Slave Device ID 0 Sensor ID
//Sensor physical ID
//Configures the physical I2C address of the remote I2C Slave device
//attached to the remote Serializer. If an I2C transaction is addressed
//to the Slave Alias ID3, the transaction is remapped to this address
//before passing the transaction across the Bi-directional Control
//Channel to the Serializer.
0x65,0x60, //7-bit Remote Slave Device Alias ID 0 Sensor Alias ID
//Configures the decoder for detecting transactions designated for an
//I2C Slave device attached to the remote Serializer. The transaction
//is remapped to the address specified in the Slave ID0 register. A
//value of 0 in this field disables access to the remote I2C Slave.
0x70,0x1e, //RAW10_datatype_yuv422b10_VC0
0x7c,0xe1,
0xB0,0x00,
0xB1,0x01,
0xB2,0x01,
0xB1,0x02,
0xB2,0x33,
0xB1,0x03,
0xB2,0x1e,//yuv8bit
0xB1,0x04,
0xB2,0x09,//1280*2
0xB1,0x05,
0xB2,0x60,
0xB1,0x06,
0xB2,0x01,
0xB1,0x07,
0xB2,0xE0,
0xB1,0x08,
0xB2,0x02,
0xB1,0x09,
0xB2,0xD0,
0xB1,0x0A,
0xB2,0x04,
0xB1,0x0B,
0xB2,0x1A,
0xB1,0x0C,
0xB2,0x0C,
0xB1,0x0D,
0xB2,0x67,
0xB1,0x0E,
0xB2,0x21,
0xB1,0x0F,
0xB2,0x0A,
0x20,0x00, //e0//forwarding of RX0 to CSI0
--------------------------------------------------------------------
The plot is as follows, the right side of the image is not abnormal and is parsed correctly at the set resolution.

The register values for DS90UB960-Q1 under test pattern mode are as follows:
0x0,0x7a,
0x1,0x00,
0x2,0x1e,
0x3,0x40,
0x4,0xd0,
0x5,0x01,
0x6,0x00,
0x7,0xfe,
0x8,0x1c,
0x9,0x10,
0xa,0x7a,
0xb,0x7a,
0xc,0x0f,
0xd,0x09,
0xe,0x01,
0xf,0xff,
0x10,0x91,
0x11,0x00,
0x12,0x00,
0x13,0x00,
0x14,0x00,
0x15,0x00,
0x16,0x00,
0x17,0x00,
0x18,0x43,
0x19,0x00,
0x1a,0x06,
0x1b,0x5b,
0x1c,0x9b,
0x1d,0x00,
0x1e,0x04,
0x1f,0x02,
0x20,0x00,
0x21,0x83,
0x22,0x00,
0x23,0x00,
0x24,0x00,
0x25,0x00,
0x26,0x00,
0x27,0x00,
0x28,0x00,
0x29,0x00,
0x2a,0x00,
0x2b,0x00,
0x2c,0x00,
0x2d,0x00,
0x2e,0x00,
0x2f,0x00,
0x30,0x00,
0x31,0x00,
0x32,0x01,
0x33,0x03,
0x34,0x00,
0x35,0x01,
0x36,0x00,
0x37,0x01,
0x38,0x00,
0x39,0x00,
0x3a,0x00,
0x3b,0x00,
0x3c,0x00,
0x3d,0x00,
0x3e,0x00,
0x3f,0x00,
0x40,0x00,
0x41,0xa9,
0x42,0x71,
0x43,0x01,
0x44,0x00,
0x45,0x00,
0x46,0x20,
0x47,0x00,
0x48,0x00,
0x49,0x00,
0x4a,0x00,
0x4b,0x12,
0x4c,0x01,
0x4d,0x13,
0x4e,0x04,
0x4f,0x1a,
0x50,0x13,
0x51,0x00,
0x52,0x00,
0x53,0x00,
0x54,0x00,
0x55,0x00,
0x56,0x00,
0x57,0x00,
0x58,0x58,
0x59,0x00,
0x5a,0x00,
0x5b,0xb2,
0x5c,0xb0,
0x5d,0x60,
0x5e,0x00,
0x5f,0x00,
0x60,0x00,
0x61,0x00,
0x62,0x00,
0x63,0x00,
0x64,0x00,
0x65,0x60,
0x66,0x00,
0x67,0x00,
0x68,0x00,
0x69,0x00,
0x6a,0x00,
0x6b,0x00,
0x6c,0x00,
0x6d,0x7f,
0x6e,0xaa,
0x6f,0x88,
0x70,0x1e,
0x71,0x2c,
0x72,0xe4,
0x73,0x00,
0x74,0x00,
0x75,0x00,
0x76,0x00,
0x77,0xc5,
0x78,0x00,
0x79,0x01,
0x7a,0x00,
0x7b,0x00,
0x7c,0xe1,
0x7d,0x00,
0x7e,0x00,
0x7f,0x00,
0x80,0x00,
0x81,0x00,
0x82,0x00,
0x83,0x00,
0x84,0x00,
0x85,0x00,
0x86,0x00,
0x87,0x00,
0x88,0x00,
0x89,0x00,
0x8a,0x00,
0x8b,0x00,
0x8c,0x00,
0x8d,0x00,
0x8e,0x00,
0x8f,0x00,
0x90,0x00,
0x91,0x00,
0x92,0x00,
0x93,0x00,
0x94,0x00,
0x95,0x00,
0x96,0x00,
0x97,0x00,
0x98,0x00,
0x99,0x00,
0x9a,0x00,
0x9b,0x00,
0x9c,0x00,
0x9d,0x00,
0x9e,0x00,
0x9f,0x00,
0xa0,0x00,
0xa1,0x00,
0xa2,0x00,
0xa3,0x00,
0xa4,0x00,
0xa5,0x1a,
0xa6,0x00,
0xa7,0x00,
0xa8,0x00,
0xa9,0x00,
0xaa,0x00,
0xab,0x00,
0xac,0x00,
0xad,0x00,
0xae,0x00,
0xaf,0x00,
0xb0,0x00,
0xb1,0x0f,
0xb2,0x0a,
0xb3,0x08,
0xb4,0x25,
0xb5,0x00,
0xb6,0x18,
0xb7,0x00,
0xb8,0xfb,
0xb9,0x33,
0xba,0x83,
0xbb,0x74,
0xbc,0x80,
0xbd,0x00,
0xbe,0x00,
0xbf,0x00,
0xc0,0x00,
0xc1,0x00,
0xc2,0x00,
0xc3,0x00,
0xc4,0x00,
0xc5,0x00,
0xc6,0x00,
0xc7,0x00,
0xc8,0x00,
0xc9,0x00,
0xca,0x00,
0xcb,0x00,
0xcc,0x00,
0xcd,0x00,
0xce,0x00,
0xcf,0x00,
0xd0,0x00,
0xd1,0x43,
0xd2,0x94,
0xd3,0x02,
0xd4,0x60,
0xd5,0xf2,
0xd6,0x00,
0xd7,0x02,
0xd8,0x00,
0xd9,0x00,
0xda,0x00,
0xdb,0x00,
0xdc,0x00,
0xdd,0x00,
0xde,0x00,
0xdf,0x00,
0xe0,0x00,
0xe1,0x00,
0xe2,0x00,
0xe3,0x00,
0xe4,0x00,
0xe5,0x00,
0xe6,0x00,
0xe7,0x00,
0xe8,0x00,
0xe9,0x00,
0xea,0x00,
0xeb,0x00,
0xec,0x00,
0xed,0x00,
0xee,0x00,
0xef,0x00,
0xf0,0x5f,
0xf1,0x55,
0xf2,0x42,
0xf3,0x39,
0xf4,0x36,
0xf5,0x30,
0xf6,0x00,
0xf7,0x00,
0xf8,0x00,
0xf9,0x00,
0xfa,0x00,
0xfb,0x00,
0xfc,0x00,
0xfd,0x00,
0xfe,0x00,
0xff,0x00,
Best Regards,
Amy Luo