Part Number: TFP410
Is the HSYNC/VSYNC assertion period at least 1 Tpixel, or do you need multiple cycles? If I want multiple cycles, do I have to follow VESA-CVT spec section 3.6?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TFP410
Is the HSYNC/VSYNC assertion period at least 1 Tpixel, or do you need multiple cycles? If I want multiple cycles, do I have to follow VESA-CVT spec section 3.6?
The HSYNC and VSYNC are output on one Tpixel boundaries during the blanking period(Multiple cycles are not required). The signals are latched on either rising or falling edge of IDCK.