Part Number: LM8335EVM
Other Parts Discussed in Thread: LM8335
I am using LM8335EVM to drive an off-board RFFE device using the "RFFE Register Access" section of the GUI. I am mostly having success with one exception. The off board device I am controlling has registers at addresses higher than 0x1F, but when I enter an address above 0x1F the GUI automatically changes it to 0x1F.
My understanding of RFFE standard is it supports a full 1 byte address scheme (256 registers) so I don't understand why the LM8335EVM GUI would limit it to 0x1F. Some of these registers I need to get to are well beyond 0x1F; for example 0x40, so I can't even get to that with extended writes and reads.