Part Number: SN65HVD230
Other Parts Discussed in Thread: ISO1050, SN74LV32A, SN65HVD1050, TIDA-01487
Hello,
We are using SN65HVD230DR, CAN Transceiver as below

The CAN H and CAN L differential input get distorted as frequency goes above 2kHz.
As per specification it should support 1MHz.
What should be problem?
Pin 8 (S) is connected to ground with zero Ohm, I have try with 10K with also but not improve.
Please Look into this.
What should be the problem?