Other Parts Discussed in Thread: DS90UB953-Q1
we use two ov2740,raw10,2lane,720Mbps/alne,1080p60 and two ti953 works at none sync mode,the ext osc is 50Mhz,STP cable;ti954 works at 1.6Gbps and line interlaced, the ti954 can output two images, the VC channel is 0x2b0 and 0x2b1, but it seems that the number of rows is insufficient, the number of columns is correct,and when i set the reg of ti954 0x20 with 0x20 or 0x10,the output image is correct,when config 0x20 with 0x00,it seems that the number of rows is insufficient, the number of columns is correct;so i would know
1 : two sensors can work freerun or must sync ?
2 : as no refclk input at ti954,how it can work at 1.6Gbps? if it can work at 1.6Gbps, In CSI-2 non-synchronous clocking mode the DS90UB953-Q1 uses the CSI-2 clock for a reference. The
(CSI_CLK) the FPD-Link line rate is typically CSI_CLK × 10, FPD3_PCLK = 1/4 × CSI_CLK and back
channel rate is set to 10 Mbps. For example with CSI_CLK = 400 MHz, line rate = 4.0 Gbps, FPD3_PCLK =
100 MHz, the back channel data rate is 10 Mbps. When using the non-synchronous CSI-2 clocking mode, the
user must be certain the CSI-2 source meets the stringent jitter requirements for the serializer reference and
the CLK lane is always active. FPD-Link line rate equal 8Gbps ?
3: how dose ti954 merge the two image to one ? if use line buffer it means the two sensors must work sync ?