Part Number: TS3DV642
Hi TI Teams,
The notebook project, SOC has only one DP interface, but the output has two TYPE-C ports and both of them need to support DP protocol. Can we use TS3DV642 to achieve this?
If yes, I also have the follow questions:
1) The two TYPE-C ports, respectively defined as C1 and C2. When one of them was connected, whether the insert detection logic was completed in TS3DV642 chip without the SOC participation?
2) What information does the I2C of TS3DV642 need to communicate with?
Thanks,
Kind Regards