This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Teams,
The notebook project, SOC has only one DP interface, but the output has two TYPE-C ports and both of them need to support DP protocol. Can we use TS3DV642 to achieve this?
If yes, I also have the follow questions:
1) The two TYPE-C ports, respectively defined as C1 and C2. When one of them was connected, whether the insert detection logic was completed in TS3DV642 chip without the SOC participation?
2) What information does the I2C of TS3DV642 need to communicate with?
Thanks,
Kind Regards
Hi,
Please see this simplified block diagram.
TS3DV642 will not able to support the Type-C normal and flip orientation, this will have to be done by the TUSB546 or TUSB1046.
For Type-C, you also need PD controller to negotiated DP Alt Mode over Type-C.
The SOC, base on the PD controller negotiation, need to drive TS3DV642 SEL1 and SEL2 when one of them is connected. But it also needs to determine the priority if both are connected.
Thanks
David
Hi David,
Thanks a lot. But we still have one question about the voltage level of the PHD, we want to know the level is high, low, or high resistance when the switch is off ?
The circuit design of HPD terminal is as follows:
Thanks,
Kind Regards
Hi,
When switch is disabled (EN = L), all channels are in Hi-Z state.
Thanks
David