Part Number: SN65MLVD3
Hello,
The customer said that there are many broken devices. Please help analyze the cause. Thanks!
The attached file is the problem report。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65MLVD3
Hello,
The customer said that there are many broken devices. Please help analyze the cause. Thanks!
The attached file is the problem report。
Hello,
Looking at the PowerPoint slides and the previous post, it seems the issue is an overstress event, especially if it's happening to all devices. The damage occurs with the receiver's input and driver's output pins which is linked to the 4 pin Molex connector. Please ensure the correct TVS protection diodes are used to avoid going over the devices absolute maximum ratings.
Regards,
Josh