Part Number: DS25BR440
Other Parts Discussed in Thread: DS15BR401, DS15BR400, DS25BR400, TDP0604, DS25CP104A
Hi Team:
there is a new redriver application opportunity in TV video Signal Protocol --CSPI , it is specially used in Big size LED TV Panel and located in the middle place of the TV panel board, the CSPI protocol is similar with LVDS, But it is specially differ from LVDS due to 1: higher transmission data rate up to 2 Gbps, 2: the differential signal is 1.8V. so could you help to proposal a solution used in TV SOC to panel's redriver.
just attached the statement of CSPI- A Chinese protocol, thanks very much!
Point-to-point+transmission+protocol-CSPI+for+thin+film+transistor+liquid+crystal+displays.pdfTCL+CSOT+CSPI+TECHNOLOGY.pdf.