This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: the connection request of RST (Pin 32)

Part Number: DP83826E

Hi PHY Expert Team

In customer's design, they want to control the RST pin with the MCU, is there any request for the connection? Cause I see in the DP83826 EVM reference design, the RST can be connected to GND through 470 Ohm resistor. Should a resistor added between the PHY PIN and MCU PIN? Should the MCU's GPIO set as push-pull or open drain? what's the internal pull up resistance's value of PHY RST PIN?

Thank you

Joe

BR

11042022