This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB935-Q1: 935 cannot access local device via remote I2C

Part Number: DS90UB935-Q1

Hi Expert,

Our customer use 962 + 935 in MP. But recently they find many pcs failure in mass production, about 50pcs. They check and find 962 cannot access EEPROM and sensor located on 935 side. They can access 935 and configurate 935. But they have some problem access other device.

Situation1: T means the delay time between after finishing 935 config and access sensor. Now they set T as 10ms. One the failure module, they cannot test 935 I2C_SDA/SCL changing. The failure module fails 100% when power up at 21℃. But if they heat up the module to 100℃ and power on, it works properly. With the temp drops down to 21℃, it always works well. 

Situdation2: based on situation1, they adjust the delay time T to 750ms. And they test 3 modules and all works well. They will test more. 

Attached is 935 reg dump. Please help analyze. You can also check internally if we have similar issue before. This case is really urgent. They already have 2000 cars held off. Thanks.

935 mutiregs-20221112.xlsx

BR,

Elec Cheng

  • Hello Elec,

    - Which I2C strap voltage are they using on the SER?
    - Why are they using different values for register 0x8C? This is controlling the internal LDO value! They should not touch this!
    - Can you provide two register dumps from the DES connected Port. One dump in working case and other dump from NG case?

  • Hi Hamzeh,
    Which I2C strap voltage are they using on the SER?

    It's very weird that they only config 935 register as below initial code. They don't change 935 register. And I also compare 935 register between good and bad. You can see my screen shot as below.  The left one is bad and right one is good. The only difference between them are the several "reserved" register. Can you share more details about these reg? I am also asking the customer whether they change them or not.

    935 initial code:

             {0x02, 0x73},

             {0x0d, 0x00}, /* disable remote gpio */

             {0x0E, 0xA5}, /* enable gpio input */

             {0x06, 0x43}, /* DIV:4, M:3 */

             {0x07, 0x7d}, /* N:0x7D */

    Can you provide two register dumps from the DES connected Port. One dump in working case and other dump from NG case?

    I compare 962 with good and fail. The difference is as below. I ask the customer to read three time for both 935 and 962, under both good and bad working. The reg is attached. I don't see much difference causing the issue, which is remote I2C doesn't work. Please help look into this case since there are 2000 car held off. Thanks.

    reg good 962 bad 962
    0x47 0x00 0x02
    0x4e 0x0c 0x04
    0x53 0x02 0x03
    0x7b 0x02 0x00
    0x7a 0x01 0x00

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/138/0602.reg-dump-1112.7z

    BR,

    Elec Cheng

  • Hello Elec,

    reg    good 962    bad 962
    0x47      0x00          0x02 -- This bit will be set if the BCC Watchdog Timer expires while waiting for a response from the Serializer while the BCC I2C Slave is active.
    0x4e      0x0c         0x04 -- In good, CSI errors reported
    0x53      0x02         0x03 -- Temo sensor
    0x7b      0x02         0x00 -- CSI error counter
    0x7a      0x01         0x00 -- ECC1 error

    All these dumps are from Rx Port2. Is the correct? All other ports are working fine?

    Can you try changing 935 reg ister 0x0A[1] from 0 to 1, and see if that resolves the issue?

  • Hi Hamzeh,

    Can you try changing 935 reg ister 0x0A[1] from 0 to 1, and see if that resolves the issue?

    Yes we already tried to change Watchdog Timer to 50ms but it doesn't work either. 

    All these dumps are from Rx Port2. Is the correct? All other ports are working fine?

    The failure follows 935 module. They test 962 connected to two 935 module. One is good and one is bad. They switch 935 module and it follows with 935 module. 

    It's very weird that they only config 935 register as below initial code. They don't change 935 register. And I also compare 935 register between good and bad. You can see my screen shot as below.  The left one is bad and right one is good. The only difference between them are the several "reserved" register. Can you share more details about these reg? I am also asking the customer whether they change them or not.

    Could you please explain the reserve register meaning? I suppose it's not our customer that changes them. Have you ever seen the reserved register changed? 

    Also we have another test today. We connect 962 with our 953 EVM, but we replace 953 with faulty 935. We have sensor on the EVM board. We also find the problem, which is 935 remote I2C doesn't output. as you can see below, at "2s" we power on 953 EVM. After 935 power up, we will run 935 initial configuration as mentioned above, and then will access sensor via remote I2C. But we cannot access it. There is no I2C output.

    Also, we put the module in -40 temp ambient and then put in 25℃ ambient for 10mins, then power up. The test waveform is as below. 935 I2C not only has no output, but also have voltage drift. 

    We will have on-site test with the customer. If there is still no progress, I am afraid that I have to set up call to discuss the problem. It's a very urgent case because the OEM hold off 2000 car because of this problem. You can also tell me what else you need for analysis. Thanks for understanding.

    BR,

    Elec Cheng

  • Hello Elec,

    I have asked this question earlier but did not get an answer from you!

    Which I2C pull-up voltage are they using on the SER?

    Can you also send me the initialization Code they are using to initialize our SER, including delays and the used sequence.

  • Hi Hamzeh,

    For 935 mode pin, it's pulled down with 10k. So the mode should be CSI-2 Synchronous mode.

    Already answer here! 

    935 initial code:

             {0x02, 0x73},

             {0x0d, 0x00}, /* disable remote gpio */

             {0x0E, 0xA5}, /* enable gpio input */

             {0x06, 0x43}, /* DIV:4, M:3 */

             {0x07, 0x7d}, /* N:0x7D */

    935 initial code is here. There is all for 935 initiation.

    As I said, we need your strong support here since it's very urgent case. Thanks for understanding!

    BR,

    Elec Cheng

  • Elec,

    please read my question carefully! you have not answered it .

  • Also, I have talked to the team about this behavior. They are pretty sure that this has to do with the WD timeout. Please refer to the attached document and make sure the customer implement and test this correctly!

    5732.FPD-Link Camera Startup flow.pdf

  • Hi Hamzeh,

    The pull up voltage is 1.8V. You can see below schematic.

    BR,

    Elec Cheng

  • Okay thank you!

    Please be aware that the recommended pullup resistor on I2C = 4.7 kΩ for the Standard and Fast mode, while a pullup resistor of = 470 Ω is recommended for the fast plus mode. However, the pullup resistor value may be additionally adjusted for capacitive loading and data rate requirements as per this AppNote.

    But as I said, I have talked to the team about this behavior. They are pretty sure that this has to do with the WD timeout. Please refer to the attached document and make sure the customer implements and test this correctly!

  • Hi Hamzeh,

    Thanks for your recommendation here. We set "Speed up I2C Bus Watchdog Timer" as 50ms both in 935 and 962 and it works fine. But for this issue, we have several confusion regarding to our test today.

    1. what's the difference between "Speed up I2C Bus Watchdog Timer" and "BCC_WD_TIMER"? We only change "BCC_WD_TIMER" to a small value and it doesn't work. Is "BCC_WD_TIMER" also related in this case? 

    2. Currently we the register setting is : "Speed up I2C Bus Watchdog Timer" is 50ms. "BCC_WD_TIMER" is 10ms. Is it good config? 

    3.. "Speed up I2C Bus Watchdog Timer" is indeed related for this issue. But from our understanding, the watchdog timer is used for reset I2C when it's not in good state. In our faulty scenario, the remote i2c is accessible 1s after PDB. So that means remote i2c enters "fault" state once PDB pulls high. Only after watchdog timer expires and pull remote i2c back to good state. So why would it act like this? Is it normal?

    4. As we mention and test today, with setting "Speed up I2C Bus Watchdog Timer" as 1s. It tends to easier to appear in -40℃. We test one module and it works fine in 15℃ and doesn't work in -40℃. The customer test many module and find in -40℃ it have a higher failure rate. So why is it related to temp? What does temp affect? 

    Thank you, Hamzeh again for help in this case!

    BR,

    Elec Cheng

  • Hello Elec,

    glad to hear it is working fine!

    what's the difference between "Speed up I2C Bus Watchdog Timer" and "BCC_WD_TIMER"? We only change "BCC_WD_TIMER" to a small value and it doesn't work. Is "BCC_WD_TIMER" also related in this case? 

    BCC_WD_Timer is only for the communication between SER and DES, and it allows termination of a BCC transaction if it fails to complete within a programmed amount of time.

    But I2C_Bus_WD_Timer is responsible on the local I2C bus in the Camera, which could be free or hung up following an invalid termination of a transaction.

    Currently we the register setting is : "Speed up I2C Bus Watchdog Timer" is 50ms. "BCC_WD_TIMER" is 10ms. Is it good config?

    Please change the BCC_WD_Timer to higher than the 50ms. I would change it to ~100ms.

    "Speed up I2C Bus Watchdog Timer" is indeed related for this issue. But from our understanding, the watchdog timer is used for reset I2C when it's not in good state. In our faulty scenario, the remote i2c is accessible 1s after PDB. So that means remote i2c enters "fault" state once PDB pulls high. Only after watchdog timer expires and pull remote i2c back to good state. So why would it act like this? Is it normal?

    If UB935 detects activity on I2C bus on power-up, it will go into a 1s timeout during which transactions to other slaves connected to 935 are inhibited.
    Timeout is based off an internal clock (which can vary by up to +/-40%). Which means during power-up, I2C transactions may be inhibited for up to 1.4s.
    Since I2C is based on open-drain IOs, any power supply transients on the power supply will directly translated as activity on I2C and detected as activity by the SER and will trigger the timer. This is especially true during the start-up as there are current transient during device power-up.

    Transients due to in-rush current will be detected as I2C activity at startup and can trigger the watch-dog timer.

    As we mention and test today, with setting "Speed up I2C Bus Watchdog Timer" as 1s. It tends to easier to appear in -40℃. We test one module and it works fine in 15℃ and doesn't work in -40℃. The customer test many module and find in -40℃ it have a higher failure rate. So why is it related to temp? What does temp affect? 

    The Temp change will affect the internal Oscillator clock which can vary as said up to +/-40%, which means in time variation of 600ms to 1.4s. Also, different temperature may have an impact on the power supply for faster or lower rise and fall times.

  • Hi Hamzeh,

    Thanks for your reply!

    Please change the BCC_WD_Timer to higher than the 50ms.

    Could you please explain why BCC_WD_Timer should be higher?

    Since I2C is based on open-drain IOs, any power supply transients on the power supply will directly translated as activity on I2C and detected as activity by the SER and will trigger the timer. This is especially true during the start-up as there are current transient during device power-up

    We understand that the I2C controller enters time out due to transient or disturb on the I2C bus. From your point of view, is it often the case? Is it normal in customer's system? And I am curious that why I2C  watchdog timer is default as 1s? 

    The Temp change will affect the internal Oscillator clock which can vary as said up to +/-40%, which means in time variation of 600ms to 1.4s. Also, different temperature may have an impact on the power supply for faster or lower rise and fall times.

    In one test, we measure it takes about 2s from the PDB pulls up to remote I2C access. Is there any more possible cause that will extend the time? 

    Another question, to address the problem before we set I2C watchdog timer to 50ms, the customer will make I2C retry till finally access. In normal operation, do we need the retry still? Thanks.

    BR,

    Elec Cheng 

  • Hello Elec,

    Could you please explain why BCC_WD_Timer should be higher?

    If "BCC_WD_Timer" is the same or lower than the "I2C Bus Watchdog Timer" then every time the I2C Bus timer is waiting for a response, the BCC will be terminated which will create double problem; local I2C termination and BCC termination. To avoid the BCC termination, it is recommended to increase its timer as I said.

    From your point of view, is it often the case? Is it normal in customer's system? And I am curious that why I2C  watchdog timer is default as 1s? 

    Yes, we have seen other customers with the same implementation which leads to timeout, hence we have created this AppNote to help customer avoid this behavior if they can't keep their I2C bus clean once our device comes out of PDB.

    You are right, the default is 1s to allow more time before terminating the local I2C bus transactions, but this can be changed to 50ms if the customer wants a faster system startup.

    In one test, we measure it takes about 2s from the PDB pulls up to remote I2C access. Is there any more possible cause that will extend the time? 

    This can happen if the WD_Timer was triggered 2 times after each other.

    Another question, to address the problem before we set I2C watchdog timer to 50ms, the customer will make I2C retry till finally access. In normal operation, do we need the retry still?

    Retry mechanism is always good. In case the WD Timer is triggered two times after another (but this may happen very rarely though), then this would help.

  • Hamzeh,

    I work with Elec together for the case.

    Customer need to explain to CAR OEM so they still need more clarification from TI.

    One thing we cannot explain is why this phenomenon goes with our specific silicon UB935 (A-B-A swap experiment done). 

    And the issue can be easily reproduced at low temperature with this specific UB935 (around 10% UB935 can have this behavior at low temperature like -20C).

    Bad UB936 can reproduce the phenomenon at our EVM at -20C.

    Could you give us a technical explanation for us to report to CAR OEM to close the issue?

    Thanks

  • Hi Hamzeh,

    Besides Ryan's question, I have another request. As you may know, this case causes great influence for both CAR OEM and Tier-1. From my point of view, to better close this case, it would be the best if you can provide a material, such as app note or technical manual explaining the root cause and how changing the register helps on technical aspect, to the customer to serve as a conclusion. You can send us via e-mail since this is public forum. Thanks.

    BR,

    Elec Cheng

  • Hello Team,

    this is not a device issue. As explained in the App note I have provided earlier, this is a system implementation issue.

    The different behavior at different temperatures, should be coming from other devices as per the provided Appnote.