Part Number: THVD8000
Dear TI team,
we are planning to use the THVD8000 in our designs as a cost-efficient alternative to our G.hn 2-wire communication.
In this context, a couple of questions appeared.
Here are the two most important for us at the beginning:
1.) Since our G.hn design (and HD-PLC as well) is running with long-range 48V DC power supply (and slightly above) , we were wondering if and how we have to change the design compared to the EVM or data sheet or design guide. Are there things we have to take into account? Or do the propsed design work for higher voltages as well?
2.) It would be great to have the OOK communication with the OFM of G.gh on the same bus. As we are going to run OOK with 500kHz and G.hn usees the frequency band of 2-200Mhz, it should be basically possible. What we see when trying to run both on the same bus is, that G.hn communication stops working, OOK is not reliable anymore. Any suggestions for that or did you ever had a similar request?
Thanks for an answer in advance.
Best regards
Alexander W. Lenhardt