Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: DS90UB948-Q1
Dear community,
I am working with DS90UB947-Q1(Serializer) and DS90UB948-Q1(Deserializer). The bouth are configured to work in single FPD-Link 3 mode. It works well in the single FPD-Link 3 mode.
I have to configure the bouth to wirk in dual FPD-Link 3 mode. From the data sheet, I have configured the bouth as follow:
DS90UB947-Q1:
register:
0x5B = 0x82.
DS90UB948-Q1:
registers:
0x34 = 0x09
0x49 = 0x00
For the DS90UB948-Q1 I check the configuration with 0x1C register:
0x1C = 0x13
the DUAL_RX_STS is set, but DUAL_TX_STS is not set.
For the DS90UB947-Q1 I check the configuration with 0x5A register:
0x5A = 0xCD
The configuration look good in the Serialiser.
But in the Deserializer the DUAL_TX_STS is not set.
I write the configuration, but nothing is happend. They continue working in the single FPD-Link mode.
Do I do something wrong or I miss something in the configuration.
Best Regards,
Iordan.