Part Number: SN65LVDS100
Hello,
I need to implement AC coupling on the inputs of the SN65LVDS100 LVDS repeater (based on figure 50 in its datasheet). If the SN65LVDS100 is off (as the rest of the board) and there is activity on the LVDS lines, it is possible that negative voltages will be present on A and B inputs.
1-Is this acceptable?
2-If not, can you recommend a protection circuit?
Thank you