This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: RGMII-to-SGMII bridge mode

Part Number: DP83869HM

Hello All,

This is regarding a custom board wherein we are using the part DP83869HM. We have an RGMII interface on a microprocessor and SGMII interface on a switch. We want to use this PHY as a bridge between the two.

However, the RGMII interface is at 1.8V and the SGMII is at 3.3V. Please find the below query regarding the same:

Does supplying only VDDIO with 1.8V suffice for the same in two-supply mode. Or is it necessary to opt for three-supply mode for the same?