Part Number: SN65LVDT14-EP
SN65LVDT14-EP is now being used on AC inverter. Customer would like to evaluate the thermal. Could you kindly offer Theta_JC and T_junction Temp,max ?
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVDT14-EP
SN65LVDT14-EP is now being used on AC inverter. Customer would like to evaluate the thermal. Could you kindly offer Theta_JC and T_junction Temp,max ?
Regards
Brian
Hello Brian,
Below are the thermals for the SN65LVDT14-EP:
| Theta JA | 86.1 °C/W |
| Theta JC (Top) | 28.4 °C/W |
| Theta JB | 37.2 °C/W |
| Psi JT | 1.4 °C/W |
| Psi JB | 36.8 °C/W |
For max junction temperature (TJ(max)) this is 150 °C. See [FAQ] What is the maximum junction temperature (TJMAX) for a device?
Regards,
Josh