Part Number: THVD1400
Hi, For the part THVD1400DRLR - the ESD Values in the Datasheet are given as 16KV for Bus Terminals and 4KV for All other pins.

In order to consider ESD, which value should be considered "All Other Pins" or "Bus Terminals"?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1400
Hi, For the part THVD1400DRLR - the ESD Values in the Datasheet are given as 16KV for Bus Terminals and 4KV for All other pins.

In order to consider ESD, which value should be considered "All Other Pins" or "Bus Terminals"?
Hi Rohith,
Clemens is correct - bus terminals are A/B and everything else is "other". So there is more robust protection on the Bus Pins (as in many RS-485 applications the bus pins are the ones that are more likely to be exposed to the outside world which would give more chances for larger ESD events).
Best,
Parker Dodson