This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN55LVDS31-SP: SN55LVDS31-SP: Function Table 1 still has two G Enables, no Gbar

Part Number: SN55LVDS31-SP

As pointed out here, Table 1 of the datasheet has an error in which both enable columns are designated 'G'. There is no 'Gbar'. The chosen resolution to the linked question stated that the datasheet update would be put into the queue for the next revision of the datasheet. It's been four years and this has not been fixed.

  • Hello William,

    It seems this datasheet update was not properly queued into our system. I will submit a request to update the graph in Table 1. Due to our datasheet revision process, please allow a couple of weeks for the changes to appear on our website. Thanks.

    Regards,

    Josh