This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65MLVD206B: Receiver Output Glitch on DE Transition

Part Number: SN65MLVD206B

Several years ago a question was asked regarding glitches on the receive output pin of a receiving node when DE transitions from high to low (https://e2e.ti.com/support/interface-group/interface/f/interface-forum/126882/help-with-noise-on-a-half-duplex-m-lvds-line) on a transmitting node.  The last post by Earl Close describes my exact same situation with the SN65MLVD206B.  My setup is exactly the same.  My bus cabling is 100 ohm twisted shielded pair with 100 ohm termination on both ends.  *RE is permanently asserted on all nodes.

When a node is finished transmitting, the data is logic low (this is our stop bit).  When DE is de-asserted (high to low), we see a very brief glitch on the R pin (which should be logic low) of the other nodes on the bus.  At the DE transition, we see both A and B lines begin their transition to a floating state, but for a very brief amount of time, A rises slightly above B causing the logic high glitch on the R pins.  We tried to add a resistor bias network on the bus to pull A low and B high during idle, but found that we had to implement this on every node right at the device A and B pins.

Just wanted to re-post the issue to see if there might be any suggestions of what could be happening.

Below is the original question posted in the now closed thread:

I am having the exact same problem as Luis. I am using the 65MLVD206 and tried briefly with the 65MLVD201 to see if it was better. My setup has a transmitter at one end (switched on and off via TE), 10 cm of transmission line, and a receiver at the other end. *RE is tied low at both ends. Each end has a 100 ohm terminator.  I need R at the receiving end to look exactly like D at the transmitting end. I will show you what I found on the scope:

1: signal at D on transmitting 65MLVD206

R2: signal at R on receiving 65MLVD201 (not really usable)

2: signal at R on receiving 65MLVD206 (this has the glitch when TE is turned off)

R1: signal at DE on transmitting 65MLVD206

Zooming in on the glitch on the R line (the bottom trace):

and looking at the LVDS A and B lines:

1: signal at D on transmitting 65MLVD206

R1: signal at B on receiving 65MLVD206

2: signal at A on receiving 65MLVD206

From this you can see that the LVDS signals behave. When TE is turned off, the B signal rapidly drops, and the A line moves up slightly but still B>A so we should not see a 1 output.

It seems if I go to a 50 ohm termination instead of 100 ohm the problem goes away. I can also bias as Luis did, but it seems something is fundamentally wrong. I want a robust solution, and I fear this is a band-aid solution.

Are you able to explain what is happening? Does the receiver have some inductance such that when B drops rapidly with A rising that it sees this as a 1, even though the voltage levels don't justify this?

Thanks,

Earl

  • Hello Patrick,

    Thanks for bringing this to our attention. Let me ask another peer on why this is exactly happening.

    In the meantime, based on Earl's post, are you able to confirm the glitch disappears if the 100 ohm termination resistor is replaced with a 50 ohm resistor at both ends?

    Regards,

    Josh 

  • Hello Patrick,

    We are still trying to figure out why this glitch occurs. We ordered the EVM for this device to see if we get similar results.

    Were you able to confirm if switching the 100Ω termination with a 50Ω termination fixes the glitch issue? Are you able to provide waveforms?

    Regards,

    Josh

  • Hi Josh,

    Thank you for looking into the issue.  We have tried other termination values, but we quickly run into issues with reflections if we move too far away from 100 ohms.  I have not attempted to re-create this same issue at 50 ohms.  I also do not have waveforms captured and we have already modified our boards with resistor bias networks.  I know that is not much help, but I can say that the information Earl Close posted is pretty much identical to the things we observed. 

    I am curious if you will see what we saw with the EVM.  We had 6 nodes on the bus, and each node was a different cable distance from the other.  I could take some measurements of our cable lengths if you were going to try to re-create the configuration.

    -Patrick

  • Hello Patrick,

    On your first post you did mention having a 100Ω twisted pair cable. Since the termination resistor and the cables characteristic impedance don't match then reflections will happen. I was just curious if the solution Earl mentioned would work on your setup as well.

    Please allow 3 - 5 days for us to receive the EVM and the 206B device from our storage facility. We will try to replicate the glitch based on your and Earl's post. I should be able to provide an update by next week. Thanks.

    Regards,

    Josh