This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does the DS110DF410 and DS250DF410 support these features?
1、Does TI's retimer guarantee that the input Serdes signal is at the same frequency as the output Serdes signal?
2、Does the chip implement the following functions internally: restore the input serdes through CDR, debounce through the internal PLL, and then send it to the corresponding output port to generate a serdes signal?
Hi Aiwen,
I suggest reading this section from the datasheet which should answer your questions.
Best,
Lucas
Hi Lucas;
This messege does not specify whether the output signal is exactly the same as the input signal frequency .it just describe the way of Debounce and VCO frequence setting , could you please Check it out again?thanks!
Hi Aiwen,
The output signal frequency is the VCO frequency, which either locks to the mean arrival times of bit transitions of the input signal or is manually set by the user. In both cases the output signal is only present if the VCO frequency is locked to the input signal, so yes the output signal frequency is the same as the input signal frequency.
Best,
Lucas
Hi lucas;
Does DS250DF410 is similar to DS110DF410 that output signal frequency is the same as the input signal frequency.
Hi Aiwen,
Yes, all of our retimers and redrivers have the same output signal frequency as input signal frequency.
Best,
Lucas
Hi lucas;
Very grateful for your reply, There is still another question here, Could you please help to confirm it ?
DS250DF410: Does it support the following 4 optical modules?
1、100G: Does 100G C2M support CAUI-4 (baud rate: 25.78125GBd) and GAUI-4 (baud rate: 26.5625GBd)?
2、50G: Does 50G C2M support LAUI-2 (baud rate: 25.78125GBd) and GAUI-2 (baud rate: 26.5625GBd)?
Hi Aiwen,
The Typical Applications section of the datasheet shows examples of DS250DF410 supporting both 100GbE and 50GbE front-port applications. The datasheet also specifically mentions support for CAUI-4. I would expect DS250DF410 to also support the other 3 optical modules assuming the signaling requirements are similar to CAUI-4.
Best,
Lucas
Hi Lucas;
DS250DF410 and DS250DF810 rate 25.8G, what are the limitations compared to the DS280DF810 (28.4G)?
Hi Aiwen,
These are the key differences between these 3 parts:
Best,
Lucas
Hi Aiwen,
No, they are very similar devices that operate with different data rate ranges.
Best,
Lucas
Hi Lucas;
1、DS250DF810, DS250DF410 are used in 100G CR scenarios (DAC cable 100G out of the panel), how many meters are the actual successful application cases cable?
2、Does the DS250DF410 support the following modes: host -(25.78125GBd NRZ *2lan)-retimer(DS250DF410)-(26.5625GBd NRZ*2lan)-module(QSFP28)?If not, is there a suitable reference design recommendation?
Hi Aiwen,
It's difficult to give a specific reach for DAC cable applications because it depends greatly on the insertion loss profile of the cable used. If you have a model for the cable you are considering, I can provide an IBIS model for DS250DF410 so you can simulate the link.
I believe your second question has already been answered in the following thread: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1194106/ds250df410-supported-optical-module-question
Best,
Lucas