Other Parts Discussed in Thread: DS90UB960-Q1, DS90UB933-Q1, DS90UB935-Q1, DS90UB913A-Q1, DS90UB962-Q1,
hi team,
please tell difference of 960/962/964
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi team,
please tell difference of 960/962/964
Hello,
Thanks for reaching out.
The main differences between the 960, 962, and 964 are the following:
DS90UB960-Q1:
-Supports up to 4 Cameras with a maximum line rate of 4.16 Gbps/Camera.
-Two CSI-2 output ports
-Compatible with the DS90UB935-Q1, DS90UB953- Q1, DS90UB913A-Q1, and DS90UB933-Q1 Serializers
DS90UB962-Q1:
-Supports up to 4 Cameras with a maximum line rate of 3 Gbps/Camera.
-One CSI-2 output port
-Compatible with the DS90UB935-Q1, DS90UB953- Q1, DS90UB913A-Q1, and DS90UB933-Q1 Serializers
DS90UB964-Q1:
-Supports up to 4 Cameras with a maximum line rate of 1.9 Gbps/Camera.
-Two CSI-2 output ports
-Compatible with the DS90UB913A, DS90UB913Q, and DS90UB933 Serializers
Regards,
Kenneth