Part Number: DP83869EVM
Other Parts Discussed in Thread: TEST2,
Hi Team,
I have one Question here .
refer above link this product can work in 10/100/1000 Base-T Ethernet speed .
Lets consider below setup
PC1 --> DP83869EVM1 ( configure in 1000 / 100 Media converter mode ) --> 1000Base-X SFP --> optical cable --> 1000Base-X SFP --> DP83869EVM2 ( configure in 1000 / 100 Media converter mode ) -- PC2
Test1 - PC1 in 1G Ethe Speed PC2 in autoNeg. mode ( 1G speed detected) ( both EVM in 1000Mbps Media Converter configuration )
Test2 - PC1 in 100Mbps Eth speed PC2 in AutoNeg. Mode ( 100Mbps speed detected ) ( both EVM in 100Mbps Media Converter configuration )
Test 3 - PC1 in 10Mbps Eth speed PC2 in Auto Neg Mode ( not work ) Please suggest Configuration setting .
can above all 3 test run successfully Automatic without any config change ?
i have seen that some media converter avalable in the market if you change speed in one side ( PC1 ) then speed automatiocly change another side ( PC2 ) and no need to implement any configuration change , they have manage some how internaly
is this DP83869EVM can do the same ? if yes please suggest the configuration setting .
Regards,
Nikunj