Part Number: DP83TD510E
Other Parts Discussed in Thread: DP83822I
Hi Ti Team,
We have developed a SPE to Ethernet Media Converter based on the DP83TD510E and DP83822i both operating as RMII Slave operating of a 50Mhz Oscillator.
JPerf tests show great data rates over both TCP and UDP ~ 9.5Mbs, no loss of packets and Network Jitter of ~ 2ms over a 1km line (CAT6 twisted pair)
Our application is using Audio UDP and Video streaming via TCP - UDP Audio packets are sent every 10ms at 160 Byte payload plus IP overhead.
We found that UDP Audio was fine although once we included the Video stream through the link our Audio was effected by packet to packet Jitter/Latency of ~ +/- 10-15ms observed in Wireshark and audibly noticeable.
Total Bandwidth being used didn't make any difference, initially we were using a total of 7mb/s, then we reduced it to a total of 2.7mb/s and the Jitter/Latency was still present.
Once we remove the video stream the Jitter/Latency results come good +/- 0.5ms.
If we removed the SPE Cards and replaced them with a Netgear 10/100mb Switch the Jitter/Latency results were also good with Audio+Video +/- 0.5ms.
Can SPE address anything around latency or is this addressed on other network layers I.e Application using buffering.
Wanted to confirm if there was anything we could check on our prototype design before we go to market.
Kind Regards,
Daniel