Part Number: SN65DP159
We are having issues with HDMI 2.0 data rates on a custom PCB that uses this component. Any screen resolution / frame rate combinations that result in a data rate < 3.4Gbps are working just fine. However, whenever we go into data rates > 3.4Gbps I am getting no output from the HDMI. The screen flickers black for a moment, then the embedded software on the board reports the HDMI TX stream has gone down. The stream comes back up shortly after and the process loops endlessly.
I have tried the same monitor / cable on a development board containing the same FPGA SoC, and HDMI 2.0 rates are working just fine on there. So the issue definitely lies with the new custom board.
Here are the register dumps from the working case on this board (< 3.4Gbps) and the non-working case (> 3.4Gbps):

Can you provide guidance for further investigation into this issue?
Thanks.