Part Number: DP83867CS
Other Parts Discussed in Thread: DP83867E
Hi Team,
When my customer did compliance test of their DP83867CSRGZR board under 10Base-Te, the compliance test results became as follows,
I would appreciate any advice on their compliance test results.
In addition, the results are the same as the e2e test results below.
1.e2e URL
e2e.ti.com/.../dp83867ir-10base-te-100base-tx-1000base-t-compliance-test
2.10Base-Te Test results
- 2 fails at the following items,
1) TP_IDL Template, with TPM (last bit CD0) : Fail at Load2
2) TP_IDL Template, with TPM (last bit CD1) : Fail at Load2
3.10Base-Te Test condition
(1)Test fixture (10Base-Te with TPM):640-0581-001 (EEE-TPA-ERK)
・The above is a test board dedicated to 10Base-Te.
(2)Test PatTern
・at 10BT TEST,Since the link partner cannot output pseudo random,
the pseudo random signal by the PHY BIST (0x16) function was used as the test signal.
◆Below, register settings
0x1f 0x8000, PHY RESET
0x00 0x0100, 10Base-T / Te mode
0x10 0x5008, Forced MDI mode
0x16 0xd804,
(3)oscilloscope:KEYSIGHT
I found a thread related to this issue on the E2E community, but I'm not sure if it was resolved.
Please tell me the following points.
<Question1>
As per the forum answer below, I tried to write the GPHY register.
-------------------------------------------------------------------------------------------
2. For 10BTe :
a. Measure TP_IDL on load 2 (where it was failing earlier) with following extra configuration :
reg<0x009F> = 0xCCCC.
--
Regards,
Vikram
-------------------------------------------------------------------------------------------
By implementing the above settings, the amplitude increased by 0.2V.
Also, the TP_IDL template (LOAD2) now passes.
But it failed with 10BASE-Te peak differential voltage.
・Measured value: 2.129V
・Pass limit: 1.540V <= VALUE <= 1.960
Is it possible to finely adjust the differential amplitude of 10BASE-Te?
Is there any other way to increase the output level?
<Question2>
It was reported that the e2e community and the DP83867 EVM had similar results.
Please let me know the compliance test results of the DP83867 EVM so that I can compare the results.
<Question3>
Has the E2E community issue below been resolved?
e2e.ti.com/.../dp83867ir-10base-te-100base-tx-1000base-t-compliance-test