Part Number: ONET1151L
Hi,
could you please provide me the formula for the digital BMF and PMF fault register threshold settings?
In my setup I am e.g. testing the following for BMF in open loop:
BIASPOL=1 => 1/70 => Ibias=0.12mA*ADC=17.87mA
BIASC=200, MODC=0, OLENA=1
When I lower BMF I get the laser turned off when BMF reaches 46 and can be turned on again at 47 by toggling ENA.
How can I relate the 8bit BMF=46 to the measured Ibias by the 10 bit ADC?
And is the difference between the BIASC=200 set Ibias=200*102uA=20.4mA and the measured 17.87mA normal?
In my setup I am also testing the following for PMF in closed loop:
BIASPOL=1,PDRNG=01, MODC=0,OLENA=0
APC enabled and set to 1mW laser power by tuning BIASC
Ipd=2.6uA*ADC=410.7uA
When I lower PMF, I get a laser power fault at 61 and am able to turn the laser on again at 93.
Can you provide me the formula to compare both and an explanation for the large difference between turn off and turn on values?
Is the PMF threshold e.g. triggered by an overshoot of the laser power when turning on again?
Cheers
Philipp