Part Number: DP83867E
Hello,
Looking back at this thread:
I performed the steps necessary:
For this setup, PHY A and PHY B will be connected via RJ-45. Assuming these are configured correctly, they should link up. This should be checked via Reg 0x1[2]. If this is set up correctly, then you may enable setup testing by enabling PRBS on PHY A while PHY B will be set to Reverse Loopback. You may then check errors via Reg 0x72, number of received bytes in 0x71, as well as PRBS status on 0x17.
and it is not working. May I ask what I should do?
Thanks.