Part Number: SN65DP159
Other Parts Discussed in Thread: TCA9517A, TCA9509, TCA9517, TCA6507
Hi, David.Liu:
I have a new finding, and let's continue the below thread:
I connect Aardvark I2C/SPI Host Adapter to IIC chain as below figure shown, and DP159 could be accessed successfully through it . So, I turn to this level shift(TCA9517ADGKR) and guess this LS
maybe block access of DP159, especially the low level signal which make the DP159 could not identify the device address.

Below figure shown the waveform through this LS without Aardvark I2C/SPI Host Adapter . The low level is close to ~500mv which accord with 0.52mv(VOL) in the datasheet. I can't see the ACK from DP159


Below figure shown the waveform through Aardvark I2C/SPI Host Adapter. The low level is close to ~250mv. Also I can see the ACK from DP159

But, there is a strange point. The MAX VIL for DP159 is 0.3 x VCC which is 0.99v. Because 0.99v >0.6v(MAX VOL from LS), it should have be OK for access through LS. But it not.

Could you please suggest me another level shift which could be pin to pin compatible with TCA9517ADGKR?
Thanks in advance!!!
Best regards!
Jason