Part Number: DS160PT801
This question is related to the following post:
Are there conditions where the retimer can have a separate reference clock from the Root Complex?
For example, maybe if the refclk is 100MHz meeting the PCIe refclk specs and without spread?
We've been operating this way. Our architecture does not allow for a common-refclk.
It seems this spec for the chip changed around end of Q3 or 2022.
If there is some bounding conditions that we could test for, that may be an acceptable solution for us. For example SKP sequence parameters or total error between Root refclk and Retimer refclk.
Thanks,
Tony