Part Number: MAX3232
Hi,
MAX3232 output waveform is abnormal (waveform distortion), as shown in the following figure. Please help analyze the cause.
Thanks!



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3232
Hi,
MAX3232 output waveform is abnormal (waveform distortion), as shown in the following figure. Please help analyze the cause.
Thanks!



Hi Jeno,
Clemens is correct - you have unidirectional diodes that seem to want to bring the rail to ~0V when driver outputs a negative value (which is expected). You need bi-directional protection devices so that both positive and negative signals can be transmitted over the line.
Best,
Parker Dodson