This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
MAX3232 output waveform is abnormal (waveform distortion), as shown in the following figure. Please help analyze the cause.
Thanks!
Hi Jeno,
Clemens is correct - you have unidirectional diodes that seem to want to bring the rail to ~0V when driver outputs a negative value (which is expected). You need bi-directional protection devices so that both positive and negative signals can be transmitted over the line.
Best,
Parker Dodson