This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: About Lock status

Part Number: DS90UB936-Q1

Hi,

Recently, I got some logs from some fielded devices. 

The logs show that the lock status (0x4D[0]) was changed to 0 from 1 and changed to 1 in a very short time.

The register reading is triggered by GPIO3/INTB. Please see the following logs, the value in the brackets[] is in seconds:

2023-03-15T09:38:18.659823-05:00 kernel: [ 839.914369] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:38:18.663845-05:00 kernel: [ 839.917600] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:38:36.383821-05:00 kernel: [ 857.637384] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:38:36.387848-05:00 kernel: [ 857.640330] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:40:15.231825-05:00 kernel: [ 956.484223] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:40:15.236126-05:00 kernel: [ 956.487832] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:40:28.184029-05:00 kernel: [ 969.437112] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:40:28.187829-05:00 kernel: [ 969.440443] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:40:33.647832-05:00 kernel: [ 974.897651] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:40:33.647845-05:00 kernel: [ 974.901067] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:40:34.947852-05:00 kernel: [ 976.199564] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:40:34.951831-05:00 kernel: [ 976.203683] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:40:34.983827-05:00 kernel: [ 976.236640] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:40:34.987820-05:00 kernel: [ 976.240530] ds90ub954 2-0030: rx0: LOCKED
2023-03-15T09:40:35.195880-05:00 kernel: [ 976.446342] ds90ub954 2-0030: rx0: NOT LOCKED
2023-03-15T09:40:35.199835-05:00 kernel: [ 976.449555] ds90ub954 2-0030: rx0: LOCKED

We think it's because the quality of FPD-Link is not good, but we don't have any strategy to solve that.

The device worked well before this happened.

Could you help to give the possible reasons for the sympton?

Any suggestion is appreciated.

Thanks.