Part Number: DS90UB949-Q1EVM
Other Parts Discussed in Thread: USB2ANY, ALP
I am using DS90UB949-Q1EVM serializer (Device ID: 0x18) with DS90UB926 Deserializer (Device ID: 0x5A) which is connected to DLPC3030 in S32K platform(Device ID: 0x36), the Image projection part is working fine. But we are not able to connect to the i2c remote slave i.e , S32K platform(Device ID: 0x36) . We tried to write the Slave ID[0] register 0x07 and Slave alias ID 0x08 as our Remote Slave address 0x36, but communication is not happening.
code: This is our code. I2C communication to remote slave.