Part Number: DS90UB964-Q1
dear cindy
Hi Raymond,
Thank you for the clarification on the schematic.
I noticed in the register configs that you have continuous clock mode turned off in register 0x33. For debugging purposes, can you try enabling continuous clock mode and then measure the CSI clock output on the scope to see if it is still drifting in frequency?
For the register dump of the issue unit (bad.txt), what do you mean by "the failed machine reads at the time of replay?" Were these registers read when the CSI clock reached the high frequency and the screen went black?
Are these units tested over temperature, or were these measurements taken at room temp?
Regards,
Cindy
-------------------reply to this topic
As something wrong with E2E paltform display,reply as below
1. Try changing the value of register 0x33 to 0x03 and turn on continous clock mode.
2. Bad Txt inside the value of the CSI clock frequency is high, the video screen black when the export of
3, the test is carried out at room temperature