Part Number: PCA9555
The PCA9555PWR has the following address pins;
A0 = HIGH
A1 = LOW
A2 = LOW
The first write access results in a NACK. We have tried all address options from the microcontroller and it still gives a NACK.
The start and address look correct. See the attached images.
We tried standard and fast I2Csetting in the micro controller - both fail.
Standard had 10k pull-ups and fast had 3k3 pull-ups.
The power supply ramp time appears to be acceptable and there are no glitches.
I have got screen shots from the oscilloscope.
This is holding up the project.
Below screenshot is I2C using 10k pullup, standard setting in the DSP.
Below screenshot is I2C using 3k3 pullup, fast setting in the DSP.
Below screenshot is the power supply ramp period.
Here is the schematic, only the DSP, power supply and I2C bus. Note, the second I2C device (LTC2991) is working fine.