Part Number: SN65DSI86
Dear team,
Custome's application is 2880*1800, 24bit, @60Hz, pixel clock 652.26MHz, panel EDID.
Could you pls check if SN65DSI86 could support this application? Thanks!
2880 x1800 x 24 x 60 = 7.5Gbps < 1.5Gbps x 8lanes =12Gbps, so it could satisfy?
With PCLK of 652.26MHz, and 24bpp, the stream bit rate is 652.26x24= 15.654,
DSI CLK frequency = 15.654 / (2 x DSI lane). If using DSI lane of 4, DSI CLK = 1956.75MHz. ?
Thanks!