Part Number: TCA9535
Hi sir,
We interface the TCA9535 with LPC55S16 and Configuring the PORT 0 as Input. A switch is connected in P0_1 pin of TCA9535 (Where the switch has verified in both Pull-up and Pull-down). I want to identify the instant of switch press. But there is no change in INT pin status to identify the change in IO pin. How to identify the change in status of INPUT pin and how we can utilize INT pin kindly navigate us

Hi,