Hello ,expert
When taking EMI experiments for the ADAS ECU, 1.6GHz noise level exceeded the RE test standard,
Using the spectrometer test it , 1.6GHz noise can be detected between the 953 and connector.
Now 953 is connected to an external 50M oscillator, which works in non-synchronous mode
and output DVR signal from ADAS ECU to the 960 in external cockpit controller.
The question is:
1,Please tell me the method of spread spectrum for the 953 and the opposite 960 .
2,The PCB trace of the 953 FPDlink is on the bottom layer, can I layout the FPD link trace in inner layer to improve EMI performance?
thang you.
Jasper Zheng