Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4551-Q1, TCAN4550
Hi,
Good Day. I found several posts on the difference between the TCAN4550-Q1 and TCAN4551-Q1.
But my customer has some clarifications about the difference. Please see below.
I have just one extra doubt related to the differences which are not mentioned in the forums and it is almost not noticeable within the datasheet: TCAN4550 has GPIO1 but TCAN4551 has GPO1; is that right? Doesn't TCAN4551 have any input pin? Not that we are thinking now about a case where we would need it in our application, but we are considering the differences.
I also have a hardware design question. We are going to use a 2-layer PCB. The top layer has all components and routing and the bottom layer is going to be almost fully flooded cooper ground:
1. Should we also flood the top layer with Cooper ground?
2. Components on the top layer, will have each, one via to connect to the ground bottom layer to reduce inductance. Should the flooded cooper gound on top also connect to the top vias?
Best Regards,
Ray Vincent