Part Number: TMDS1204
Other Parts Discussed in Thread: DS125MB203
Hi,
We use the tmds1204 between the HDMI connector and the FPGA.
We acquire non-FRL sources up to 4K60Hz, but we can't acquire an 8K30 source despite various adjustments of equalizations/vod for both TMDS1204 and FPGA. However, the SIGDET_OUT signal is at low level and all 4 lanes output the signal.
However, the SCDC_SINK_CONFIG Register (Offset = 31h) is indicating 0x30 and we're expecting for it to be set to 0x34.
Could you help us configure the tmds1204 correctly to acquire FRL sources?